This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Headphone Detection - Leaving Mic Plugged In

Other Parts Discussed in Thread: TPA6132A2

With the latest generation of headphones having removable cords it is possible to remove headphones from a mobile device while leaving the cord in the mobile device. Normally these cables have a mic embedded in the cord which is used to detect whether headphones are present. A switched jack is used to detect the presence of headphones while detection circuitry determines whether they are stereo/mono and with/without microphone.

My question is, is there a way to detect the presence of the headphones being removed from their cord while the cord is still connected to a mobile device? I saw in one app note from Maxim that they use "an inaudible AC waveform output on the jack pins to sense when a load is plugged in" on their MAX97236 (datasheet, pg.13), but that is the only bit of evidence I have to go off of. 

I am currently using TI's TPA6132A2 headphone driver and I'd like to implement this headphone detection feature. Thanks in Advance!

-Drew F. 

  • Hi Drew,

    Information about headset detection is in this application note:
    www.ti.com/.../slaa454.pdf
    However the TPA6132A2 doesn't has detection circuit. You may need a codec from the TLV320AIC family.
    But I'm afraid that on-the-fly change of accessory type is not supported.
    I'll look for a similar application and will tell you if I find something.

    Best regards,
    Iván Salazar
    Texas Instruments