Hi:
I'm trying to evaluate the use of a PCM1804 for use as an input for a bare metal app on a Raspberry Pi.
I constructed the circuit for the single ended to balanced converter as described in the datasheet except I used three of the opamps in the quad OPA4134's for each stereo channel. I then put them through the PCM1804 circuit suggested in the datasheet. The problem is that on my scope I see the least most significant 16 or so bits are filled with noise at 192k and the least most significant 8 or so bits at 32k. In looking for noise problems I shorted the inputs to the first circuit and powered the circuits with batteries +9v and -9volt. Still had the noise. When I run a audio generator into it at 1khz I can see each bit turn on as I advance the input level once I get to the noise level and continue smoothly until all bits are filled and the overflow is indicated.
Circuits were constructed with surface mount to dip converters and point to point wiring. Used the tantalum, ceramics, and film caps suggested in the datasheet and on-board lm7805, lm7905, and ld1117 3.3v regulators and fxo-hc53 series 3.3v oscillator running at 24.576mhz. My frequency counter confirmed the lrck line was running at 191.998khz and bck was running at 12,287,835hz.
I would appreciate any suggestions on what and where to look to find the noise source and any suggested solutions.
Wes Brenner