Other Parts Discussed in Thread: PCM4202
I'm having problems with this 4202 part on another new product design.
Running in slave mode, 48K sample rate, so FS0,FS1,FS2, FMT0, FMT1, HPFD are all tied to GND.
SCKI is 12 MHz (256FS) and BCK is 6 MHZ (128FS).
It seems I can get the ADC in a mode where the noise level jumps like 40db up from spec/baseline level. We first noticed this just doing some random testing. Since then, I've poked around some more and made the following observations.
If the 4202 is operating as expected, I can heat board up and all is still good.
If I get my can of freeze mist and chill the 4202 a little bit, still good. If I chill enough to get frost, I can here brief intervals of noise jumping up and then calming down as the frost transitions to water.
If I do this frosting cycle a few more times, I can get it to where the ADC gets into this noisy mode and stays there. If I force a reset (this requires my FPGA to do a full reprogram cycle which kills all clocks, restarts clocks and then releases reset), the noise clears up and all is good again.
This text from spec page 16 is a little puzzling to me.... I'd like to know what sensitivity issues they are talking about.
The BCK rate is typically equal to 128fS in Single Rate sampling mode, and 64fS in
Dual or Quad Rate sampling modes. Although other BCK clock rates are possible, they
are not recommended as a result if potential clock phase sensitivity issues, which can
degrade the dynamic performance of the PCM4202.
I have this part running on other designs that happens to be running at 64Fs BCK rate and haven't had an issue as yet.