Other Parts Discussed in Thread: LM49450
Looking at the LM49450 specification for Vih on the digital inputs, I read a minimum of +2.8V is required.
However the datasheet also says that IOVDD can be as low as +1.8V: “IOVDD powers the I2S and I2C, allowing the LM49450 to interface with lower voltage digital controllers”.
So that +2.8V requirement does not make sense and should instead be a percentage of IOVDD.
Could you Clarify whether there is a different Vih specification?
Another related question.
Making the lower limit of IOVDD +1.8V is confusing because that does not really include a +1.8V supply.
To be able to power IOVDD with a typical +1.8V regulator/supply, the IOVDD spec should be >= +1.7V to account for the regulator/power supply variation.
Any chance LM49450 can actually be specified for an IOVDD >= +1.7V ?
Thanks For the Help,
Lucas McKeehan