Other Parts Discussed in Thread: LM833, LM833-N
A look through the more recent data sheet issues for this device have thrown up a couple of questions...
In the TI data sheet 'SLOS481B –JULY 2010–REVISED OCTOBER 2014' for the LM833, fig 8.2, the functional block diagram clearly shows the output stage as being a quasi complementary using two NPN devices. This is at odds with 'SNOSBD8E –MAY 2004–REVISED MAY 2012 ' for the LM833-N and also at odds with old data sheets going back through the history of the device which show the standard complementary emitter follower pair.
This 'difference' (if it is a real production change) would make significant changes to the devices performance, perceived and actual.
Any clarification on this would be appreciated.