Other Parts Discussed in Thread: PCM5242
Hi All
I want PCM5142evm to work in i2s master mode.
I set GPIO3 as input ( i am providing 20 MHz clock externally) , set PLL clk source select as GPIO , set GPIO src for PLL reference as GPIO3 and set GPIO6
as output.
I enable PLL ,set the register dividers for 90.316 MHz output and set GPIO6 output selection as 10000b (PLL/4).
Now i should see some clock at GPIO6.
I get some random sine wave. Please suggest what I am doing wrong?
I will pass this signal at SCK and then program BCK and LRCK using dividers.
Thanks and Regards
Ankur