Other Parts Discussed in Thread: SRC4382, SRC4392
Hi all,
I am using an SRC4382 as sample rate converter for AES3 and/or S/PDIF. Now I want to use some GPO (GPO1 and GPO3) to show what is happening.
To do this I have hooked up LED's to each of these pins in sourcing mode (with series resistors).
The LED's are not showing anything, this could have two reasons:
1. The GPO are sinking IO.
2. The GPO cannot supply enough current (LED requires 2mA)
The datasheet of the SRC4382 and the SRC4392 does not say anything about the electrical characteristics of the GPO other than "IO = –4mA" and "IO = 4mA".
I'm not sure how to interpret this info, can anyone clarify this for me? Datasheet page 4 of the SRC4382.
Greetings,
Justin