Other Parts Discussed in Thread: PCM1804, OPA2134, OPA134
1. My customer has searched other applications and found many supplied the OP amp with +/-5V in front of many high-performance ADC. And he sketched me his intended circuit as follows. However, I believe the PCM1804 receives VIN that swings in the 0~5V range. Because the positive input(accordingly the negative input as well) to the OPA2134 is biased by VCOM of 2.5V. See page 30 of the PCM1804 spec. OPA2134 portion is depicted as if it is supplied by +/- voltages. Please advise quickly if blow sketch makes sense. They prefer using a +5V only.
2. The customer wants recommendation for a small yet good performing OP amp. Will OPA134 work?
3. What is the problem when the PCM1804 AVDD is supplied with 3.3V? Any trick to use such way?