Hi All
I am trying to use LM4675 PA to create human voice. I got the following questions:
1. In this case, I want to use single ended input mode, which IN- is connected to the signal input while IN+ is connected to GND through a serial RC components. Can I use a PWM signal generated from MCU such as CC3200 to retrieve the human voice? The illustration of problem is plotted below.
2. There are two outputs of LM4675 which are Vo1 and Vo2. Should Vo1 be connected to the "+" of 8 ohm speaker and Vo2 connected to the "-" of 8 ohm speaker? Or polarity of speaker does not matter?
Thanks
Heng