This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5538 Loudness Compensation

Hi,

Could you please give us your advice regarding the loudness compensation as below ?

Q1. Maximum of Peak Gain
Would you tell us the maximum of the peak gain for the loudness although we understood that the bass and treble tone controls with +/-18dB range ?
Please tell me the gain to be saturated in the internal processing.

Q2. Gain Setting of 0x93
The peak gain is 15dB if setting the loudness function parameters, then the value of 0x93 is 0080 0000.
Is our understanding correct although we believe that the peak gain will be 3dB if setting 0002 0000 to 0x93 ?

Q3. Total Gain
The gain is the input signal 8 times(18dB) if mixing the 8channel input.
Is it possible to connect the biquad filter to the next stage with 18dB ?

Best regards,
Kato