Hello,
I designed an active stereo organ amplifier (with build in DAC) using the TAS5630DKD fully balanced. One half of the IC does the bass and the other half tweeter. Amplifier is used in AD and BTL configuration, with 43V dc and 12V from a seperated 7812 power supply. We coursly used the TI application digramm, only little differences and off course a different layout, since it had to build inside the organ.I can provide PCB layout and pictures for reference. We use Coiltronics HC1-5R1-R chokes in the filter section and 680nF MMK capacitors. Chokes do not get really warm (40 degrees C) and also residual carrier is about 600mV, seems ok? Design is symmetrical right from the DAC outputs (PCM1795 mono mode).
Amplifier works fine, also sounds really good, but we have constant very audible whistling noises from both bass and tweeter amplifier halves, and also both channels the same. Also a little hum and quite a lot of hiss noise from the tweeter. But these also can be caused by the zero feedback and very compact design. Biggest problem is the quite loud whistling noises.
Can there be any cause for this, probably it is because of the PCB design or Hf filtering/decoupling somewhere, but as far as i can see I did everything the datasheets asked for and still have the problem. Any help would be greatly appreciated! Thanks!
Mattijs