This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi sir:
About PGA2500, I have aquestion to ask.
It is that when I try to adjust PGA2500 level shift to support the AD input range 0~5.
But it is not work. I am not sure that I control is corrected or not.
Links are described in detail below:
My application describe as below :
Microph phone + INA110 + PGA2500 + AD7988
AD7988 is single end input, so I want to adjust PGA2500 level shift to match AD7988 input range 0~5v
Thanks.
Best Regards,
Kun You Lin
Hello,
What is your desired PGA2500 common-mode voltage, +2.5V? The schematic only shows a connector on the VcomIN pin. You must remember that the VcomIN pin sets both the input and the output common-mode voltages of the PGA2500. Since you have Vin- shorted to GND, you are directly connecting (VcomIN - 0.65V) to GND which will cause short-circuit currents inside the part and most likely cause severe performance issues.
As specified in p. 13 of the PGA2500 data sheet, setting VcomIN = +2.5V causes output swing limitation and THD+N degradation. As an alternative, we propose keeping VcomIN = 0V and AC-coupling the PGA2500 output as shown in Figure 8.
Best regards,
Ian Williams
Linear Applications Engineer
Precision Analog - Op Amps