Other Parts Discussed in Thread: LM4865
Hi,
We're tinkering with the LM4865 Power Amplifier IC.
So far, no real problems, it works as stated on the datasheet.
But we do notice one peculiarity -
We're driving the Volume Control input with DC derived from a 1K pot wired between +V and ground.
We can see that the DC voltage rises and falls smoothly with pot rotation, but the output level of the
amplifier appears to change in discrete steps, not a smooth continuous change.
Has anyone else experienced this, and is it normal for this IC?
Thanks for any feedback -
SBH