This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204 bandwidth for SDR?



I am exploring using the 5535 EVM for low frequency SDR operation. It looks like all the normal setup for the 3204 limits the audio bandwidth to 20 kHz. It is not clear if it is possible to use 192 kHz sampling with Decimation filter A to give bandwidth on the order of 40 kHz. Is it possible? has anyone actually done such an unusual thing?

Thanks.