Hello engineers,
The phenomena is that the PCM2900C is damaged after the 5V Vbus provided for over 1 minutes.
-
The internal voltage is ok, I can measured 3.3V output from every LDOs.
-
About 3.1V voltage on the XTI pins instead of the oscillation.
-
The current requirement on the Vbus input is observed, 10ma in the initialization time, last more than 100mA.