I'm using the TLV320AIC3206 evaluation board and I'm getting unexpected behavior on with the AGC noise threshold.
When the the AGC and noisethreshold is on and the input is below the noisethreshold, I expect the AGC gain to be very low. It is however at maximum and the white noise is loud in the output (through the left mixer amp bypass). As you can see from the screenshots, the noise flag is set but the AGC gain is high (and output is loud). When the input is above the noise threshold, the AGC is reduced and the flag is off, as expected.
Why isn't the AGC gain reducing when below noise threshold?
Thanks for your help!
Noland