Other Parts Discussed in Thread: TLV320ADC3101, DIT4096, PCM2902C, TMS320C5533, PCM2706, PCM2706C
Hi there!
Im designing a USB digital MEMS microphone board for a large scale noise sensing project. I have the option of using the following 2 digi mics:
- ST MP34DB01 - PDM output
- InvenSense ICS-43432 - I2S output
Can anyone suggest an audio IC that can take either a PDM or I2S input and provide a USB audio compliant interface to act as a sound input device (at 44.1 or 48kHz) for a linux based mini PC?
Ive looked at solutions involving MCUs, but the extra level of complexity to get the software side up and running is offputting.
Ive been looking at the TLV320ADC3101, which can handle a digi mic PDM input, but would require a USB audio interface IC in addition to it. This is still a possibility though.
Any advice would be much appreciated!
Charlie