Other Parts Discussed in Thread: MSP430F5529, PCM1796, PCM9211
Hi all,
i am working on pcm1796 and msp430f5529.
here in pcm1796, pin ZEROL & ZEROR (pin1 and pin2) is connected to microcontroller. when I2S input comes then these pins goes low and when not connect then pins goes high.
but when i connect it with 10k Resistance to microcontroller at BIT6 and BIT7 of PORT2 then it generate pulse means interchange between high and low and when i2s input connect then it working properly.
i want to know where is the problem in pcm1796 or in connection or anything else.
2- mute function also not working.