Can I feed one coaxial S/PDIF input into the RXIN0/1 inputs of two different DIX9211s (to create a multi-zone switch)? Or is there some internal biasing that would preclude tying two of those inputs together?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I feed one coaxial S/PDIF input into the RXIN0/1 inputs of two different DIX9211s (to create a multi-zone switch)? Or is there some internal biasing that would preclude tying two of those inputs together?
Hi Dave,
There are multiple outputs for the DIX9211, and so you could output the single SPDIF input to two outputs on one DIX9211. Could you explain a little more of what your application is?
Justin