Audio Champs,
Working through the Characterization process I ran into "Unable to playback Audio" a few times during the HW Checks. It only seems to happen sometimes.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Audio Champs,
Working through the Characterization process I ran into "Unable to playback Audio" a few times during the HW Checks. It only seems to happen sometimes.
I managed to resolve this after a bit of trial an errors.
In the Windows's Sound-->Recording Menu (Right click the speaker in the system tray and go to Recording.)
1. Ensure that the "5-USB-AudioEVM" is set to the Default Device for recording
2. Ensure that the Levels is set to 100 (this can also be accomplished by maxing your volume on the speaker in the windows bottom right tray)
3. Ensure that the Default Format (in the Advanced tab) is set to "2 Channel, 16bit, 44100 Hz".
The same should be done in the Window's Sound-->Playback Menu.
Hi Michael,
Thanks for the feedback!,
Regards,
-Diego Meléndez López
Audio Applications Engineer