Other Parts Discussed in Thread: TAS5631B, TAS5162, TAS5631
Hi all,
Since 2 years we manufacture an eight channel amplifier unit using 4 pcs TAS5631B on one board. In general, specifications are ok and reliability is no issue either. However a strange phenomenon appears during production tests, specifically at THD vs freq sweeps.
In general distortion figures are low, however the odd channels have allways lower distortion figures than the even channels. There is allways one odd and one even channel in the same chip. Sometimes, one channel may have 10dB worst distortion than the others, but after a powercycle this might be changed to an other channel. A new version of the childrens game "who will take the chair" obviously. An almost identical board with TAS5162 does not exhibit this strange behaviour.
Could it be that this has to do with the re-sampling that occurs inside the TAS5631B?
regards
Geert de Vries