Other Parts Discussed in Thread: PCM1864
Hello,
I have a question about PCM1864.
SLASE55A specifies that Sampling Frequency is "32 kHz to 192 kHz" in the Table-1 of the Page-3.
Cannot I use 24kHz?
And SLASE55A specifies that Sampling Frequency is "8kHz, 16kHz, 48kHz, 96kHz and 192 kHz" in the Table-10 of the Page-33.
Can I use other frequency?
Regards,
Daisuke