This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About 100k-ohm of resistance to TPA3111D1 of AVCC 14 pin

Other Parts Discussed in Thread: TPA3111D1

Hi

My customer adopts the TPA3111D1, is being evaluated before mass production.
If my customers are the slew rate of the AVCC(14pin) is more than 10V/ms,
they knew the need for resistance of 100k-ohm.

I want you to check the attached waveform.

(1)The slew rate of the period from the GND level to 8.8V of AVCC (14pin) is 23.2V/ms.
   This value is more than 10V/ms.
(2)The slew rate of the period from 8.8V to 17.8V of AVCC (14pin) is 7V/ms.
   This value is less than 10V/ms.

Do 100k-ohm resistance is required for AVCC(14pin) in this case?

Thanks

Masumoto

TPA311D1_AVCC(14pin)_waveform.pdf