Other Parts Discussed in Thread: PCM1789
I have an application involving a PCM1789, wherein the analog supply is not always available. As presently designed, the product can run for an indefinite period period of time with the digital supplies (VDD) at 3.3V, but the analog supply floating. It appears to float to about +2V due to slight leakage from the PCM1789, held by a large bypass capacitor on that supply.
I am wondering if this is an acceptable operating condition for the PCM1789? The datasheet specifies that it doesn't matter in which order the supplies come up, which implies that it is ok at least for a short time, but I'm not sure this should be construed to mean that it can operate that way indefinitely.