Hi team,
I need to meet the following specifications for an audio speaker:
1. I2S Codec
a. Input
i. Microphone
b. Output
i. Mono
c. Features
i. Integrated power amp (3 - 6 W)
ii. Single Supply
2. I2S or PWM low power Amp
a. Output
i. 3 - 6 V
b. Features
i. Single supply
At first, I was looking into the the TAS2552, which fulfills the power amp requirement (correct me if I'm wrong here). My question is, does the TAS2552 require an audio codec between it and the processor? If it does, can you please recommend one based upon the requirements above?
After looking into that, I also found the part TAS2521, which looks to have an embedded miniDSP to take care of the codec portion of the requirements. Can this device fulfill the requirements above and integrate the codec and power amp into one IC?
Thank you!
Jared