Other Parts Discussed in Thread: TAS5710, TAS5754M
The HybridFlow 3 block diagram (and I think most of the other HybridFlows) in the "Using the TAS5754/6M HybridFlow Processor User Guide" shows the “Output Volume” control after the “DRC” block. This results in the DRC compressing the signal based on the input level. If the input level is loud the signal will be compressed even when the output volume is set low.
Is there a way to put the DRC after the volume control? For example, the TAS5710 has the DRC after the volume control which seems to make a lot more sense.
Thanks,
Kevin