Hello,
We have been using the PGA2500 in one of our products for more than 5 years without any problems. All of a sudden, on this last production run, about 2% of the chips are failing. The failure symptom is a very high (up to 4 or 5 volts) DC offset on the outputs. The chip has a fancy DC offset circuit that requires 2 external caps, but the datasheet doesn't give any details about how the circuit works. I am suspecting something like flux residue on the boards that is affecting the DC offset circuit. Unfortunately, cleaning the board with alcohol doesn't fix the problem.
Can someone give me ideas about what might make the DC offset circuit misbehave. How sensitive is it to leakage current of the external caps, or leakage current to power or ground that might be caused by flux residue?
Thanks,
Mehrdad.