This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3118D2 Minimum load Impedance

Our customer has a question about TPA3118D2
I'm posting the question for the customer:

++++++++++++++++++++++++++++++++++++++++++++++

About Minimum load Impedance of TPA3118D2;

Data sheet describes "Minimum load Impedance[RL(PBTL)] : 1.6ohm(min)" 

Our load (connecting to PBTL out) is 2.2ohm at 100Hz and less than 1.0ohm at <50Hz.
But Over-Current protection is working when we output to the load 
with High-Pass Filter with a cutoff frequency of 300 Hz.

We have one question;
 Does the "1.6ohm" mean DCR[Direct Current Resistance] ?

++++++++++++++++++++++++++++++++++++++++++++++

Thanks in advance.

Best regards,
Takishin