Dear Specialists,
My customer is evaluating LM3886.
After the test of long term test, temperature rise is increased.
He anticipated that output impedance is increased, output transistor HFE is decreased.
Is it correct?
Are there other reason?
Could you please advise which characteristic has changed.
---the customer use case---
Vcc: +24V, Vee: -24V
Supply current: 5.8Arms
Load resistance: 2.7ohm
-----
I appreciate your great help.
Best regards,
Shinichi