Please suggest me an IC to generate PWM for Class D power amplifier, the input is sine wave (10kHz to 30kHz). The need to generate PWM around 300kHz.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please suggest me an IC to generate PWM for Class D power amplifier, the input is sine wave (10kHz to 30kHz). The need to generate PWM around 300kHz.
Hi Kadagala,
Welcome to E2E, Thanks for your interest in our products!.
I would suggest you to take a look to our Audio Selection tool, it offers a great overview of our devices so you can be able to choose the right part for your application.
Can you share more information of your application?, like the part # of the amplifier that you are trying to drive, or desired output power level. This way we can help you finding the best solution.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Thank You for your suggestion.
I need to amplify a 0.5V-2V, 15kHz-25kHz input signal to 400V output of same input frequency. For doing this I need to compare the input with triangular wave (10 times of input frquency, 250kHz) and generate PWM. The PWM drive the MOSFETs in H-Bridge configuration (dc voltage 400V) and the power output is 500W. The amplifier will finally drive a transducer.
I am looking for ICs for the above application.
Best Regards,
V.S. Kadagala