Other Parts Discussed in Thread: LF353, LM358, LM386, OPA827, OPA1611, OPA172
I am looking for a starting point on how to build a condenser microphone amplifier circuit to pick up voices in a 20' by 20' room. The amplifier needs to be driven off a single supply of 24 or 12vdc. I was planning on using a Omni direction condenser microphone with a nominal input voltage of 5vdc. The microphone would pick up the voice of someone speaking in the middle of the room with enough clarity to understand the words. The output of the amplifier will be connected to an Analog to Digital converter with a voltage range from 0 to 5VDC. The AtoD chip can have 10 or 12 bit resolution and sampled at what ever interval is needed.
I have experimented with the LM358, the LF353 (Worked great but needed + &- 12vdc) and the TLC27M2CP.
Could someone point me in the right direction with a chip suggestion and a recommended amplification or gain?
I would assume I want a high gain, low noise, high voltage Op-Amp?
Thanks
Daryl