Other Parts Discussed in Thread: LM48560
Hello,
We currently use the LM48560 in two modes:
- Boost enabled with 21 dB gain
- Boost disabled with 18 dB gain
Changing between the two modes requires two register writes:
- To enable/ disable the boost: Register 0 - 0x1F (boost_en) or 0x1D (boost_en disabled)
- To change the gain: Register 2 - 0x00 (21dB when boost _en) or 0x03 (18dB when boost_en disabled)
What we have found is that when writing the two registers to perform the change, the settings do not take any effect. However, when only one register is written, the setting takes effect immediately.
We have tried all sorts of combinations of register write order, repeating the writes, event strobing /SHDN off and on for 5 ms before the register write, but none of these methods have worked and the no settings take any effect when two registers are written in succession.
Is it possible to make these settings change on the fly and switch back and forth between the two modes?
Thanks,
Chris