Hi,
As part of a Parametric Speaker prototype I am currently working on, I am planning to drive an Ultrasonic Transducers Array using a TI Class-D Amplifier TPA3111D1PWP.
An Array of 50 transducers with the Specifications below[1], arranged in a parallel mode as can be seen in an attached figure.
As a result, the Array is to be driven by 10[W] and will present resistance of 20[Ohm] and conductance of 100[nF].
Would be glad to have your advice on the following issues:
- Is the TI Class-D Amplifier TPA3111D1PWP suitable to drive such a circuit?
- If the array to be connected to OUT+ and OUT-, what are the values of the L1 and L2 to be used?
- If the array is to be connected via a Molex connector, what are the values of the FB1 and FB2 to be used?
[1] http://www.mouser.com/ds/2/209/KT-400244-193495.pdf
Thanks in Advance.