This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM48560 / to switch amplifier input dynamically

Guru 29720 points
Other Parts Discussed in Thread: LM48560

Hi Team,

Is it possible to switch amplifier input(IN1 and IN2) dynamically?
He wants to switch within 20ms.
I would like to know it for both hardware mode and software mode.

Best Regards,
Yaita

  • Hi Yaita-san,

    Yes, LM48560 is able to swap IN1 and IN2 on-the-fly.
    It takes around 13.5 mS to change between channels.
    For software mode, these 13.5 mS are counted after the I2C writing sequence is completed.
    For hardware mode, these 13.5 mS are counted after the SDA/SEL pin is changed from VDD to GND or GND to VDD.
    I hope this helps.

    Best regards,
    -Ivan Salazar
    Texas Instruments