Hi all,
several TAS devices (like TAS5711 in our design) specify rise/fall time for MCLK to be 5nSec max.
If I feed such a steep MCLK (12.288MHz in my case) into the TAS5711, PLL does not lock at all and stays at ~350kHz. Slowing down MCLK a little (at least 7-8nSec rise/fall) immediately provides a safe lock.
Other TAS datasheets do not specify rise/fall for MCLK at all or specify minimum times for high/low levels.
Is it safe to run the device with a slightly slower rising MCLK or do I have to re-check my layout or should that 5nSec from the spec rather read as a minimum time?
Thanks in advance