Other Parts Discussed in Thread: TAS5630B
Hi all-
I am experiencig a start-up issue on a TAS5630B (DKD package, PBTL mode) borad I am working on. This a revision of a previous version of the board (that performned perfectly) where minor changes have been made. These changes did not involve the TAS563B routing on power sypply and output pins.
On the new board release, when feeding power, the device will start occasionally, but most of the times it will not start oscillating and SD and READY pins will remain low, even with outputs disconnected (no load) and zero input signal
Schematic and component values are identical to datasheet's reference design.
According to the datasheet's statements, the device has PPSC (chapter 7.3.5) and this was my first investigation. I have carefully checked for a possible condition that may trigger the PPSC and did not found any.
Still I belive the that the PPSC is triggered for some reasons because the device does not respond to a toggle on the reset pin.
Or maybe I am not looking in the right direction...
Any suggestion is welcome
Thanks for your support.
Marco