Other Parts Discussed in Thread: PCM1863, PCM1864, PCM1865
Hello,
I am using the PCM1863 as an ADC as well as digital input mixer. I have configured GPIO2 as a digital input, and GPIO0 as DOUT2. I have set the mixer for the I2S input to 0dB. With the 1863 configured to run at 24 bit/96k, I am not able to see any signal out on DOUT2. Other than configuring the mixer coefficients and the GPIO settings for the digital in/out, is there a register setting I am missing to make this work?
Thanks, Kris