This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5754 in master mode generating sclk and lrclk

Hello,

I am trying to output the sclk and lrclk from the TAS5754 in master mode. The only clock i'm feeding is the mclk on pin 22. I have follow the instruction of the user manual to set the appropriate register and I'm writing the value in the register via I2C.

The thing is I don't have anything on the pin 25 and 23 (lrclk and slck output) after the register set up. The mlck I use is 24.57 Mhz and I need fs of 48Khz.

Does anybody have the value of all the register needed to make this work?

Thanks