This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
I am designing the final audio amp stage for a system with a 3.4volt single supply . The input needs to be mono, single ended ~line level. Output needs to be >1 watt into 4 or 8 Ohm onboard speaker with the ability to plug in/switch to an external speaker/headset via external audio jack with no less than half power of the onboard speaker. The problem that I'm having is that the type of external speaker device required has one end of the speaker tied to ground due to other functionality within the connection and device and it is not cost effective to isolate ground or use another type of external speaker/device for this application. the TPA0233 seems just about right but a little low on power I need help with understanding some details about the TPA0233 and any other options that may be more suitible to my application. The internal speaker could use a Class-D amp but the external speaker could be up to 6' (wire length) away from the amp in addition to the speaker being ground referenced.
Can 1 single ended input be used for both BTL and Headphone modes on TPA0233?
Is there a higher wattage amplifier with functionality/Vcc similar to TPA0233 ?
Is there a simple way to capacitively couple the audio out to the ground referenced external speaker and still use a Class-AB differential amp without a headphone mode?
Should i be concerned about the distance of the external speaker as far as using a Class-D? and if not is there an efficient way to couple a Class-D to a ground referenced external speaker? If yes to these, what Class-D would you recommend?
Summary: 3.4 Volt single supply, single ended ~line level input, 1 Watt audio output required, Mono output to internal speaker "floating" 4 or 8 Ohm or external speaker - referenced to power supply/signal ground(within external speaker device).
Thanks for reading.