Hi,
Would like to get your advice on LM4865M application.
Intend to change the speaker load impedance from 8ohm to 4ohm.
Could you please advise whether it is OK to use this part based on below conditions?
DC Supply: 3.4 to 4.2V
Speaker Load: 4ohm
Speaker Power Rating: 1W (max 1.5W)
Target is to achieve 500mW at THD=1% (Bridge Mode).
Package: SOIC.
Normal ambient temperature: 25 Degree (with operating temperature is -15 to 60 deg).
Note: Based on calculation ,power dissipation seems OK.
But under LM4865 spec/performance characteristic, it does not mention this device can support 4ohm load impedance.
Is there any potential issue for this device to support the design application?
Thanks,
Phil