Hi,
I am trying to use the AIC3262 Eval board do mix the input of a digital mic connected to (GPO1 and GPI1) and the onboard MIC_IN connector (J2). I am using PPS to route these two signals to the HPL/HPR output. Currently I am able to use either the digital mic or the analog input but not in combination.
For the time being I can mix any combination of ASI#1,ASI#2, ASI#3 and the analog input.
Is there any option to use the digital mic input and the analog input at the same time and route this signals to the HPL/HPR?
regards Martin