Hi,
I just need to implement separate outputs with both channals of linout and headphone on DSK6713, but until now I only know, that the outputs in both the channels are the same. I use always the command of AIC23: while (!DSK6713_AIC23_write(hCodec, x[sample])) for example. And I know that I can change the configration settings to adjust the volume of the headphone channel, but the headphone channel and the lineout channel always output the same signals, how can I for example outputs a sine wave in the lineout channel and at the same time outputs a noise in the headphone channal. Is it possible?
best regards
Johnny