HI,
I want generate the sampling rates by using the BLCK3 and WCLK3.
I referred the TLV320AIC3262 datasheet, 2.7.2 Low Frequency Reference Clock.
1)get the clocks from host to codec is wclk=48 kHz and bclk=1.536 MHz.
2)According to datasheet LFR_CLKIN should be less than 50 KHZ.
3.here i can't use the bclk,if can use the wclk(48 kHz) then how it will work.
4. wclk is directly goes to LFR_CLKIN,LFR_CLKIN should connected to Clock Frequency Multiplier,there what about the MCLK1 and HF_OSC_CLK.
5.here MCLK1 is required,if i can use the wclk.
6.i used wclk(48 KHZ),then what is the value of HF_REF_CLK.
7.please give me the solution for above lines and explain how to use the ASI3 slave mode.
8.please share me any code base for ASI3 slave mode with LFR_CLKIN configurations.
Thanks