I have been trying to use a beagle bone black to drive the TLV320AIC3107 EVM audio chip by connecting the BCLK, MCLK, WCLK, DIN, DOUT, RESET. SDA and SCL similar to the connection in the audio. I have gotten data out of the dout port a few times but other times it doesn't work. It either hangs on the speaker test and nothing seems to be going through the BCLK, WCLK or MCLK. I assume the resgisters and settings should be handled by the codec driver?
Below is an image showing the audio cape connection and my device tree.
SCHEMATIC
AM335X Device Tree
/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/dts-v1/;
#include "am33xx.dtsi"
#include "am335x-bone-common.dtsi"
/ {
model = "TI AM335x BeagleBone Black";
compatible = "ti,am335x-bone-black", "ti,am335x-bone", "ti,am33xx";
};
&ldo3_reg {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};
&mmc1 {
vmmc-supply = <&vmmcsd_fixed>;
};
&mmc2 {
vmmc-supply = <&vmmcsd_fixed>;
pinctrl-names = "default";
pinctrl-0 = <&emmc_pins>;
bus-width = <8>;
status = "okay";
};
&sgx {
status = "okay";
};
&am33xx_pinmux {
mcasp0_pins: mcasp0_pins {
pinctrl-single,pins = <
0x1ac (PIN_INPUT_PULLUP | MUX_MODE0) /* mcasp0_ahclkx.mcasp0_ahclkx */
0x19c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mcasp0_ahclkr.mcasp0_axr2 */
0x194 (PIN_OUTPUT_PULLUP | MUX_MODE0) /* mcasp0_fsx.mcasp0_fsx */
0x190 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mcasp0_aclkx.mcasp0_aclkx */
0x06c (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpmc_a11.GPIO1_27 */
>;
};
mcasp0_pins_sleep: mcasp0_pins_sleep {
pinctrl-single,pins = <
0x1ac (PIN_INPUT_PULLDOWN | MUX_MODE7) /* mcasp0_ahclkx.mcasp0_ahclkx */
0x19c (PIN_INPUT_PULLDOWN | MUX_MODE7) /* mcasp0_ahclkr.mcasp0_axr2 */
0x194 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* mcasp0_fsx.mcasp0_fsx */
0x190 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* mcasp0_aclkx.mcasp0_aclkx */
0x06c (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_a11.GPIO1_27 */
>;
};
i2c2_pins: pinmux_i2c2_pins {
pinctrl-single,pins = <
0x150 0x72 /*spi0_scl.i2c2_sda,SLEWCTRL_SLOW | INPUT_PULLUP |MODE2*/
0x154 0x72 /*spi0_d0.i2c2_scl,SLEWCTRL_SLOW | INPUT_PULLUP | MODE2*/
>;
};
audio_pins: audio_pins {
pinctrl-single,pins = <
0x1ac 0x00 /* mcasp0_ahclkx, MODE0 | INPUT */
0x19c 0x22 /* mcasp0_ahclkr, */
0x194 0x20 /* mcasp0_fsx, MODE0 | OUTPUT */
0x190 0x20 /* mcasp0_aclkr.mcasp0_aclkx, MODE0 | OUTPUT_PULLDOWN */
0x198 0x20
>;
};
};
&lcdc {
status = "okay";
};
&i2c2 {
#address-cells = <1>;
#size-cells = <0>;
clock-frequency = <100000>;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&i2c2_pins>;
tlv320aic3x: tlv320aic3x@18 {
compatible = "ti,tlv320aic3x";
reg = <0x18>;
status = "okay";
};
};
&mcasp0 {
compatible = "ti,am33xx-mcasp-audio";
pinctrl-names = "default";
pinctrl-0 = <&audio_pins>;
status = "okay";
op-mode = <0>; /* MCASP_IIS_MODE */
tdm-slots = <2>;
num-serializer = <16>;
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
2 0 1 0
0 0 0 0
0 0 0 0
0 0 0 0
>;
tx-num-evt = <1>;
rx-num-evt = <1>;
};
/ {
clk_mcasp0_fixed: clk_mcasp0_fixed {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <24576000>;
};
clk_mcasp0: clk_mcasp0 {
#clock-cells = <0>;
compatible = "gpio-gate-clock";
clocks = <&clk_mcasp0_fixed>;
enable-gpios = <&gpio1 27 GPIO_ACTIVE_HIGH>; /* BeagleBone Black Clk enable on GPIO1_27 */
};
sound {
compatible = "ti,da830-evm-audio";
ti,model = "DA830 EVM";
ti,audio-codec = <&tlv320aic3x>;
ti,mcasp-controller = <&mcasp0>;
ti,codec-clock-rate = <12000000>;
ti,audio-routing =
"Headphone Jack", "HPLOUT",
"Headphone Jack", "HPROUT",
"LINE1L", "Line In",
"LINE1R", "Line In";
};
};