Hi,
Could you please tell us the difference between the internal circuit topology about TPA6120A2 and OPA1622 if possible ?
Best regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ivan-san,
Thank you for your quick response.
We are suggesting to replace TPA6120A2 with OPA1622 to our customer for the headphone application.
So, which of TPA6120A2 and OPA1622 is better for the sound quality if comparing them since their feedback architecture are different ?
Best regards,
Kato
Hi Ivan-san,
Thank you for your support.
Could you please also share the comparison data of the actual measurement for TPA6120A2 and OPA1622 to us if you have it ?
Best regards,
Kato
Hi Kato-san,
I apologize for the delayed response.
An overall comparison of OPA1622 vs TPA6120A2 is in the following table. OPA1622 is better in almost all specs but output current. Although if output power/current is not a main spec, OPA1622 seems to be a better/newer option.
|
OPA1622 |
TPA6120A2 |
||
Supply voltage |
±2V to ±18V |
±5V to ±15V |
||
THD+N @ 1kHz/32Ω |
-116dB |
-101dB |
||
Slew rate |
10V/us |
1300V/us |
||
Crosstalk @ 1kHz |
-140dB |
-105dB |
||
CMRR |
127dB |
100dB |
||
Output current |
140mA |
350mA |
||
Input impedance |
60kΩ |
300kΩ |
||
Output voltage swing from rail |
Positive rail |
900mV (@600Ω) |
Positive rail |
2.5V (@25Ω) |
Negative rail |
900mV (@600Ω) |
Negative rail |
2.8V (@25Ω) |
|
Available package |
10 pin VSON |
20 pin HSOP |
14 pin VQFN |
Best regards,
-Ivan Salazar
Texas Instruments
Hi Ivan-san,
Thank you for explaining a comparison analysis.
According to the data sheet I believe that OPA1622 seems to be a better option since it seems that TPA6120A2 doesn't have a short circuit protection.
Is my understanding correct ?
Best regards,
Kato