Hello,
I designed a board using your TPA3132D2 amplifier, but it isn't working:
Actually, I designed two boards using your TPA3132D2 amplifier. The first one worked, the second one, pictured above, did not. I have checked with another amplifier to make sure the new design is working properly and outputting audio from the DAC as it should by probing the input to your amplifier chip and it is, so your chip is malfunctioning for some reason.
I also had two of these boards professionally manufactured and neither function so it's unlikely to be an issue with any solder bridging.
Here is the schematic and layout of the version which is not working:
And this is the schematic and layout for the version which did work:
As you can see the only significant change I made was to the gain setting resistor to set the amplifier to 20db.
You can also see from the photo above the chip is in the correct orientation. And I have a good 12V power supply for it.
Any suggestions how to fix this?