Other Parts Discussed in Thread: TAS5706B
Question: I am using the TAS5706B in my solution and it is working well. It does exhibit a small pop at power-up. In my system the PVDD comes on before any of the other power supplies (IE: DVDD). Can you suggest a solution without using a power sequence? I know that it is possible to improve this with a power sequence, but that can be expensive.
Answer: Yes, there is a simple fix for your concern. Simply make a voltage divider comprised of an 18K resistor from your 3.3 V logic supply in series with a 15K resistor to ground. Connect the center point of these two resistors to VR_ANA, pin 14 on the TAS5706B. Doing this will place a 1.5V bias on VR_ANA. Decouple the VR_ANA pin with a 0.01uF capacitor placed close to the VR_ANA pin. Also, the above mentioned voltage divider should be placed as close to the VR_ANA as possible.
Regards,
Fred