This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Special concerns for loads when using class-D amplifiers



1. Does Filter-free class-D amplifier need the inductance of speaker to produce audio? Or IOW, if the speaker has the characteristic as a idea resistor, can Filter-free amplifier works well?
Yes, audio contents are still present in the square waves. Your efficiency might hurt a little as Iidle is higher. There is no purely resistive speaker.

2. If we need to pay attention to the inductance of speaker when we choose a speaker for Filter-free amplifier?
Not really, you might get slightly higher efficiency with higher inductance, but I doubt you can see much improvement in efficiency above 10uH.

3. Is there any hearing difference when using speakers with different inductance?
Not with filterless Class D. If speaker L is higher, it will exhibit a higher impedance at higher freq and might affect your audio a little at high freq.
It is more important to obtain the impedance response of the speaker (i.e. Z vs freq) than to just look at a specific number like L.

4. Can I add an external inductor or ferrite bead to increase inductance of speaker in order to improve the performance.
Bad idea, anything extra that you add will introduce more loss and distortion. You should only add extra components unless they serve a specific function (eg. EMC, ESD, snubber).

 

-d2