A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
FAQ: When running the AIC23 GUI, an error message will pop up saying "privileged instruction". ?
Answer: You are running a older version of the AIC23 GUI which will not work on Windows NT, Windows 2K or Windows XP. You must run version 2.0 or later to operate on Window NT type operating systems. Also, verify that you reboot the computer after installing the GUI.