Other Parts Discussed in Thread: PCM1865, PCM1864, PCM1863
Hi TI experts,
I am studying the features of the ADC ( PCM1863 ). I hope It can work fine for my system efficiently with its features.
I have some analog input to a ADC to obtain I2S signal and I need to route the I2S signal to other applications in the same time. And I also want to input I2S signal to ADC. So I want to know deeper about the DIN and DOUT 2 features of PCM1863.
Case 1 : In master mode : Analog input and MCLK is provided externally, Let PCM1863 generate BCK, LRCK, and Data to DOUT_pin.
Questions 1 : According to the spec, I can obtain through GPIO 0 or 1 or 2 or 3 pins by set it as DOUT 2 while DOUT is in used ?
Questions 2 : If above function is available, can I also obtain the BCK & LRCK for DOUT 2 by routed them from BCK & LRCK output pin while DOUT is in used with the clocks ?
Questions 3 : If Analog signal is input, Can I obtain the data from DOUT_pin & DOUT 2 through GPIO,1,2,3 at once and and obtain the BCK & LRCK for DOUT 2 by routed them from BCK & LRCK output pin while DOUT is also used with the clocks ?
Case 2 : In master mode : NO analog input, but I2S Data input only through GPIO 0 as DIN , and MCLK is provided externally
Question 1 : Can I2S data input through GPIO 0 or 1 or 2 or 3 pins by set it as DIN and I2S data output through DOUT_pin , meanwhile the BCK & LRCK is generated internally by provided external MCLK ?
Question 2 : If above function is available, will the DATA, BCK, LRCK be synchronised correctly ?
Question 3 : If the I2S data is input to GPIO 0 by set it as DIN, Can I obtain the data from DOUT_pin & DOUT 2 through GPIO 1,2,3 at once and and obtain the BCK & LRCK for DOUT 2 by routed them from BCK & LRCK output pin while DOUT is also used with the clocks ?
I appreciate your advice, have a good day.
Fai